This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

选型咨询



现在项目需要一个输入12V,输出负5V的电源IC,请问是否有不需要外围器件的解决方案,或者有什么别的推荐?

  • 你好,

    如果需要简洁的解决方案,推荐使用TPS71550,TPS76050,TPS76150,TLV70450。这些方案只需要外接1-2颗电容就能实现,如果对输出纹波要求不高可以去掉电容。

    如果电源的输出功率较高,推荐采用Buck电源。外接器件较以上方案复杂。

    TI的解决方案众多,可以在www.ti.com.cn/.../power_portal.page 通过选型工具选择合适的方案。

  • 你好,注意到你需要的是负5V的输出,用一般LDO做解决方案的话需要将芯片地接到-5V电势上,因此输入电压需要大于17V。二楼推荐的TPS71550和TLV0450都满足要求。

    另外还要根据实际的负载需求来具体选择。