Part Number: BQ25505
根据BQ25505的规格书利用电阻ROV1和ROV2控制电池的最大充电电压为3.1V,将ROV1设置为7.62MΩ,ROV2设置为5.38MΩ。当电阻焊接到电路板上后用万用表测量的阻值比实际值小,若将电阻与芯片断开连接则阻值恢复正常(此过程电路板未上电),实际充电时电压大于3.1V后仍然继续充电,有什么解决方法?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,The OV resistors are the only ones that affect OV termination/regulation. The only other termination/regulation issue we have found is with noise injection on VSTOR pin, which is the reason for the CBYP noise filtering capacitor needing to be placed close to IC VSTOR.
您好,有两种可能的原因。请参考下面的内容:
If the 0.01-0.1uF VSTOR cap is not placed as close as possible to IC, switching noise can cause regulation issue. The other more likely cause is parasitic resistance from residual solder flux as explained in the datasheet layout section. I recommend removing the megaohm sized resistors, cleaning the board and then reinstalling them standing or their side are replacing them with 10-50x lower sized resistors to confirm that is the issue.