Part Number: BQ24725A
我们的电池是4串的电池,需要用BQ24725A充电,设计电路是发现下面2个问题,请相关技术人员帮忙解答下,谢谢!
1、 根据线路典型应用和EV板上面都描述,使用BQ24725A时,需要MCU给芯片进行配置,设定好ACOK和IOUT,后芯片才可以工作。我的疑问是,如果MCU对BQ24725A配置好后,将ACOK和IOUT断开,(3.3V任然有),此时BQ24725A还能正常工作么?
2、ILIM脚是用3.3V分压,来设定充电保护电流。如果3.3V电压没有了,芯片BQ24725A还能充电么?
3、典型应用中的3.3V电压是不是需要一直存在?如果没有了,此芯片会怎么样?
4、与BQ24725A连接的MCU如果休眠了,对此充电管理芯片有什么影响?