Part Number: TPS51285A
现象:5V电源和3.3V电源输出后被迅速拉倒0V,疑似被保护;
问题:目前EN1和EN2信号同时给到了电源芯片,按照规格书要求,EN1需要先于EN2上电,同时给出这2个信号是否存在问题?
问题: 5V和3.3V正常起来后又被迅速拉低到0V,可能的原因是什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
同时启动EN1/2是没有问题的,你可以尝试先给EN1,后给EN2驱动信号是否正常来验证。
测试的时候,能否将负载拿掉测试看看?
同时有没有确认输入电压是否有被拉低之类?