This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76930: CC采集的电流值不准(排除计算了误差)

Part Number: BQ76930


Dear TI:

问题:
发现在放电时,采集的放电电流与实际负载仪的电流误差有100多个ma,请问这正常吗?
如果不正常,大概需要如何调整呢?目前我没有补偿和校准这个值,用的还是采集的原始值。


期望:
电流越大,这个采集值和实际负载仪的值越大,造成电流不准。排除计算和负载仪原因。根据你们的经验,大概是因为什么呢?

谢谢!

  • 您好,请参考下面的内容

    No error is expected in the current due to it being a CC.  It will integrate, if current is constant it will be a constant value.  If it were a ramp you might expect an average value, similar with a pulse.

    A common source for a linear error is the trace or solder resistance of the sense resistor. Of course check the tolerance of the resistor used, but also check to see where your traces route; coming from the pads will typically give the best result with a 2 terminal resistor.  Using a meter you can often see a voltage difference between the board terminals, sense filter resistors, and sense resistor with a current in the board. There are 4 terminal resistors made so that the sense filter can be connected to the resistor with a low current path, these are less common but can reduce the connection error if used. 

    You may note the CC has a 1.5% full scale gain error, so if you replace the part there will be some difference, but I would expect the result to be similar.  If you have other boards you might compare results and see if the result is dependent on the unit, board or resistor variation. A calibration per board is a good practice, using a low current is usually a relatively low current is suitable since the CC is typically linear over most of the range beginning to curve near the end points.