TI E2E 英文论坛海量技术问答的中文版全新上线,可点击相关论坛查看,或在站内搜索 “参考译文” 获取。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28740: 输入电压提高时MOS管驱动出现超窄脉冲问题

Part Number: UCC28740

用UCC28740设计的多路反激开关电源如下图,输入电压350-700VDC,输出电压主反馈5V,变压器Lp=1.8mH, Np:Ns=24,Np:Naux=10

测试在轻负载时(5V主反馈负载0.7A,其它路轻载或空载,输出功率约5W),母线电压提升到400V以上时开始出现如下左图驱动超窄脉冲(正常脉宽1.4us,窄脉宽<300ns),电压进一步提高后窄脉冲出现频度增大,最后会出现下右图全驱动窄脉冲现像(此时开关频率较前者有所提高)。

                        Vin:500VDC                                                                                               Vin:700VDC

CH1:Vgs(MOS) CH2:+5V

测试整改有如下现像:

1.增大CS引脚滤波的Rlc,Clc有效果。Rlc=1k, Clc由220pF->1nF后窄脉冲出现的输入电压有所提高,但无法消除。Clc小于100pF会导致电源无法启动;

2.加大环路补偿电容C22由22nF->100nF时,对窄驱动脉冲出现基本无影响。

3.测试驱动窄脉冲出现时刻的芯片CS引脚输入电压并未有异常,应该不是CS输入电压导致的驱动信号关闭

4.负载有关系,加大负载条件下(12W负载)窄脉冲出现的母线电压有所提高,配合其它参数更改如Cs>=560pF时会整个工作电压范围内都不出现。

5.调整其它参数基本上没有效果

这个问题由哪一块设计造成的目前没思路,希望大家帮忙指导下。