我想做一款交流市电输入,输出12Vdc,120W的电源,初步选择的方案是pfc+flyback,后来经过计算,发现在满载输出的时候次边峰值电流过大,现在我在PFC+flyback或者pfc+正激两种方案间犹豫,请求您们帮忙,目前我选的芯片是UCC28019(pfc),UC3842,请指教!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
或可以采用TI的UCC25600, TI有提供12V/12.5A的方案,PFC部分选择的芯片也是UCC28019, 见如下:
http://www.ti.com.cn/tool/cn/pmp4286 (这个方案有点复杂)
直接用UCC28600: 见如下方案:
http://www.ti.com.cn/tool/cn/pmp2723 这是一个12V/7A的方案,可以改到10A. (为了达到更高效率输出可以采用同步整流)
楼主如果对PF的要求不高,还可以考虑单级的Flyback PFC的方案,目前很多主流的适配器和LED公司有相关应用
我刚才一直在看您的方案,上一个方案用的是UCC28019+UCC28600来做的,是PFC+反激,后一个方案用的是交错反激,无apfc,是这样的吗?如果是,在后一个方案中如果保证pf呢?对后一个方案很感兴趣。
Hi
UC384X是比较早的芯片,TI推出方案非常少, 类似UCC28600之类芯片是TI主推的,所有有比较多的方案。
增强版本的UCC38C44有提供一个12V输出的电路,不过功率比较小:http://www.ti.com.cn/general/cn/docs/lit/getliterature.tsp?literatureNumber=slua276&fileType=pdf 并且是低输出电压的。