我有一个应用,输出的功率不大,但是要求输出的电容比较大,目前打算使用4个330uF的电容并联实现。电路打算使用TPS54160这个芯片,请问这么大的输出电容,上电启动的时候会不会有问题?如果可能有问题,应该怎么样设计呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我有一个应用,输出的功率不大,但是要求输出的电容比较大,目前打算使用4个330uF的电容并联实现。电路打算使用TPS54160这个芯片,请问这么大的输出电容,上电启动的时候会不会有问题?如果可能有问题,应该怎么样设计呢?
好的,谢谢。有两个补充问题:
1.使用的时候需不需要加大SS管脚的电容以延长软启动的时间并减小电容充电电流?
2.需不需要加大电感的电流以应对启动时的浪涌电流?
Hi
选取更大的电感的饱和电流, SS电容可以适当放大一点。