Other Parts Discussed in Thread: TPS7A7001, , TPS62130, TPS53311
目前需要两路电路 1.8V转1.0V和1.2V
有两个TPS74801和TPS7A7001
看来看去没看出来有多大区别 不知道选择哪个更优
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
反馈方式的不同控制。对于选择而言,例如如果你要想duty尽量大,选择TPS62130,因为它duty 可达100%。
所以你可以根据datasheet第一页的特性来选择芯片,但是如果要求只是电压转换,其实都是可以的。
要做比较的话,可以从效率,成本来选。