Part Number: TPS544B20
请问一下,我现在有一个TPS544B20的验证板子,请教一下该芯片是否支持通过PMbus接口动态调整输出电压?如果可以,应该如何配置?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
感谢答复,我在尝试的过程中,发现可以通过PMbus修改VREF。
我这边试验步骤如下:
1. 默认Vout = VREF *(1+R1/Rbias),硬件设计上R1=Rbias,默认Vout输出1.2V
1. VREF_TRIM设置为默认值;
2. STEP_VREF_MARGIN_LOW/HIGH为默认值;
3. 设置OPERATION[5:2]为0101(Margin Low);
那么理论上Vout = (0.6V-60mV)*(1+R1/Rbias) = 1.08V;
但是试验时发现修改后输出电压能修改到对应的1.08V,但是维持几秒后,又会恢复到1.2V。请教一下,这个可能是什么原因导致的?