想要一个大功率的pFC的方案(3KW~5KW),Vin:AC180~265V/50Hz,Vout:DC385V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
想要一个大功率的pFC的方案(3KW~5KW),Vin:AC180~265V/50Hz,Vout:DC385V
Hi
UCC28070给出的是参考设计,以及零件表,测试报告: http://www.ti.com.cn/tool/cn/pmp4311
如果你采用C2000或者MCU来做,是可以的,但是TI也没有提供5kW左右EVM板。
楼主如果对数字的方案有兴趣,也可以下载 controlsuite 获得具体的方案,主要是软件了,因为硬件的设计其实门槛很低。
controlsuite 支持中文,不过应用文档还是英文的为主,TI的应用文档也大多是英文,可以结合翻译,如果有疑问的话也可以来论坛交流
TI 提供一款300W 的UCC28070评估板。官网上可以下载到评估板的资料。
看了一下官网暂时还没有相关的方案介绍,你可以再咨询一下C2000版块的工程师确认一下-
http://www.deyisupport.com/question_answer/microcontrollers/c2000/f/56.aspx
个人了解的信息,三相PFC目前业界有应用的主要是两种都是基于C2000来做,一种是三相三开关的PFC,也是把三相输入分别经过boost做PFC,控制上与传统的PFC一致;另外一种是三相六开关的维也纳拓扑的PFC,采用的是空间矢量控制