This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我目前板上有一个19V的电源,想做一个PSE。看了很多PSE芯片都要求输入44V~57V。请问有19V输入的PSE芯片吗?或则有什么其它方式可以解决呢?
是的,根据IEEE802.AT 标准PSE的输出电压的范围44V~57V。目前没有19V输入的PSE。可能通过升压到48V,作为PSE的输入,再经过网线到PD,通过降压给负载。但升压会有一部分的效率损失,估计做成POE供电的方式,就没有什么太大的意义。
有的, 请参考TPS23756,支持12V以上的电源适配器。详见APD,PPD引脚的说明。
http://www.ti.com.cn/cn/lit/ug/slvu329a/slvu329a.pdf