This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8556物料号问题

Other Parts Discussed in Thread: LP8556

LP8556的物料号太多了。

比如我选定DSBGA封装和250颗小包装后还有:

LP8556TME-E02/NOPB

LP8556TME-E03/NOPB

LP8556TME-E04/NOPB

LP8556TME-E05/NOPB

LP8556TME-E06/NOPB

LP8556TME-E09/NOPB

LP8556TME-E12/NOPB

我看了一下手册,这些只是寄存器配置的区别,这些寄存器都是可读写的,那么是不是我就随便选个型号就可以了,反正系统初始化的时候要全部重写,或者读取/比对/只在必要的时候重写。

请确认一下我的理解是否正确。如果不正确,请推荐一下在驱动3S8P的WLED时,可能会有CABC/PWM信号,应该选用哪个物料,谢谢!

Tianfu Ma

  • 如果已选DSBGA封装,那就只有使用温度的区别:

    没有特别注明的,其使用环境为:The LP8556 operates over the ambient temperature range of -30°C to +85°C

    有些是能够在-40到85度的环境下工作的。

    对于需要CABC的,8路的可参考LP3538.