1.学习完成后,从0%开始充电,充电到100%
2.开始放电,放电到14%后,电量不在减少,这个时候:放电电流-2000A左右,电压也在慢慢下降
3.一直维持到电压低于截至电压48V后,电量跳变到0%,这个时候开始充电,电压上升后,电量从0%跳变到14%。
4.电池使用的LiFePO4电池。
5.这个不正常,由于从0%跳变到14%后,就会出现有14%的误差。
请问这个可能由什么引起的呢?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.学习完成后,从0%开始充电,充电到100%
2.开始放电,放电到14%后,电量不在减少,这个时候:放电电流-2000A左右,电压也在慢慢下降
3.一直维持到电压低于截至电压48V后,电量跳变到0%,这个时候开始充电,电压上升后,电量从0%跳变到14%。
4.电池使用的LiFePO4电池。
5.这个不正常,由于从0%跳变到14%后,就会出现有14%的误差。
请问这个可能由什么引起的呢?
谢谢!
1.SOC=14%维持不变,此时的RM和FCC是怎么样的情况?14%维持的时间有多长,一般变化1%SOC需要多长时间
2.Deadband和Dsg Current Threshold的数值是多少?
3.是否是恒流、恒功率放电DATARAM 里的Average current()和DATAFLASH里的Average current last run()的数值分别是多少?
4.放电电流-2000mA是指电量计报出来的数值还是其他仪器测量得到的
5.SOC数值是由EVSW读出的还是通过单片机等读出来,如果是单片机是否可能有其他因素导致长时间没有访问电量计寄存器的可能?
6.CHEM-ID是否有比较好的匹配?
建议贴上GG文件和log的数据