Other Parts Discussed in Thread: TPS62150A
+12V输入+6V输出 ,输出电流为0.8A
- 12V 输入-5V输出,输出电流为0.4A
效率大于92%
纹波小于30mV
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,建议可以尝试一下TI 的电源辅助设计工具WEBENCH
您好,您是想要一个两路输入两路输出的电源模块,还是需要两个电源模块。如楼上所说,webench.ti.com您可以尝试进行器件选型,使用起来还是比较方便的
Hi
正电压转换可以用TPS62150A, 满载效率高达95%,电路也比较简单,可以借组webench设计,同时带有powersaving模式:http://www.ti.com.cn/product/cn/tps62150a , 关于纹波可以参考EVM, 20mV左右。