This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq500211的SPI interface的使用疑问

Other Parts Discussed in Thread: BQ500211

  bq500211芯片有一个SPI interface,外部MCU如何和bq50021进行通信读写呢?bq500211通过该SPI会输出哪些信息?格式如何?

  • 楼主可以参考如下一个无线充电架构和通讯的介绍文档,对于初步了解无线充电产品还是有一些帮助的。

    http://www.ti.com.cn/cn/lit/an/zhct117/zhct117.pdf

  • 从您给的链接中我还是找不到我想要的答案。

    这个SPI interface会输出什么信息?要写入哪些信息?

  • 430单片机的作用是降低待机时的功耗,有430单片机,待机功耗可以做到小于90mw,没有430,只能做到300mw左右。

    开机时,BQ500211通过SPI线自动向430单片机加载相应的代码,代码实现的功能是备份与充电状态 错误信息 工作模式等相关的信息,从而避免在BQ500211掉电时丢失,且当BQ500211 shutdown时,430单片机要继续维持外部led的驱动。

    TI已经简化这个设计过程,使得BQ500211在开机会自动检测是否有430单片机 从而判断是否需要向430单片机加载对于的程序,430的代码部分用户是不能更改的。

    换句话来理解,为了简化客户开发的过程,430单片机这一块是一个已经设计非常成熟的黑盒子,用户可以不用在这方面花费精力,从而把更多精力聚焦于线路和layout的设计调试,从而降低开发难度,缩短开发周期。