This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
信息筛选显示BQ2045带HDQ通信接口,可看datasheet 没有啊?
你们的电量监测芯片‘计电量范围’在datasheet哪边有说明?BQ3055还可以计量到32000mAh?还有具备HDQ通信模式的可以计量到32000mAh的锂电芯片?
谢了!
非常抱歉给你造成困扰,BQ20z45是采用SMBus协议的,这是网页编辑上出现了一个错误。
BQ3055可以计量到32AH,因为它是基于EDV技术的,这个最大容量可以通过查阅产品的TRM(技术参考手册)中的FCC寄存器的大小体现出来。它也是基于SMBus通讯协议的。
谢了,麻烦问下TI还有可以计量到20Ah以上,HDQ通信的锂电监测芯片?
如果你是使用的单节gas gauge,可以使用BQ27541-G1.最大可以支持到32AH,可以支持HDQ通讯。