无线收发器设:接收端利用bq51013B参照《bq51013xEVM-764 Evaluation Module (WCSP Package)》进行电路板设计;发送端利用的是bq500211,参照《bq500211EVM-045 bqTESLA Wireless Power TX EVM User's Guide》,设计完成的电路板。存在问题:空载时bq500211的输出电压在0到2伏之间跳动,发送端和接收端的板子上的灯均在闪动。接上10欧姆纯电阻负载测试,调节ILIM端的5kΩ的电位器,可以将输出电压升至4.5V(此时接收端的等保持持续亮的状态),但是继续增加电压时接收端电压却跳变为0了,出现了不稳。请问这个问题怎么解决?电压到不了5V?
想咨询下无线收发正常工作时可以以5V,200~400mA左右的电流进行持续的对外供电吗?谢谢!