Other Parts Discussed in Thread: TLV1117
用7905和TLV1117搭配做了一个+/- 15V转+/-5V的电源,后面接了几个放大器,使用的时候还挺正常的,但今天上电后一摸芯片非常热,看了下电流大概有500mA,(小于手册中的最大值800mA),请问这种情况正常么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
LDO的损耗就等于输入电压减去输出电压再乘以电流,所以你每颗LDO的损耗这是5W! 我们的LDO内部做了热保护,在保护门限以下LDO还会工作。如果由于环境温度的升高,芯片内部的温升达到保护门限,则LDO会停止工作直到冷却,所以你的设计有风险。解决方法是将输入电压由15V调为6V,则损耗只有(6V-5V)*500mA=0.5W,减少到原来的10%。