This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求推荐48V输入,提供±5.5V输出的电源设计方案,纹波要小于20mV的!!!!

Other Parts Discussed in Thread: PTQA420050, PTB78560A, LP38798

我有48V的电源,需要将它转换成+5.5V和-5.5V输出,用砖形电源模块,可以多用。+5.5V需要至少75W输出,-5.5V需要至少35W输出。目前后级我是用了多组TPS78601和TPS7A3301将±5.5稳压到±5V。请大神们推荐一下中间的开关转换电路,以及模块的型号,要在上面功率输出的前提下,经LDO输出的纹波要降低到20mV以下,谢谢大家了!

PS:之前我用的是ptqa420050和ptb78560a模块,分别产生+5.5V后,然后用正接地的方法让后者产生-5.5V输出。但是这个方案在测试的时候检测到了1.5MHz的噪声(两个模块的开关频率仅低于500kHz,不解!),纹波幅度为60mV。测量方法是靠接法,限制了带宽,波形测量的方法完全没有问题。后级通过LDO能产生5V电压,但是纹波仅抑制到40~50mV之间,可能是LDO在这个频率上的PSRR太小的缘故。总之,这样的纹波直接影响了我模拟部分前级的仪表放大器的输入和输出,干扰太强了!

求解释,求推荐电路,小弟在此谢过了!

  • 你好,

    1.tps78601在100kHz-1MHz的PSRR只有20db。推荐LP38798和TPS7a8001,它们能达到40db,前者噪声更低,在精密的高速通信系统中使用广泛;

    2.看来你已经更换了开关电源模块,布板的时候开关电源的位置还是要离仪表放大器远一点,最好用金属外壳将其屏蔽;

    3.LDO的输出加磁珠,这是通信系统中常用的方法,我认为你可以借鉴。

  • 为什么不直接转换成5v呢,如果直接转换的话我们有PTQA420050隔离模块电源,功率是100W,输出5v