Other Parts Discussed in Thread: TPS7A3401, TPS84259, TPS5430, TPS5410
您好,我们现在做AD采样,需要负电压,能不能帮我们各推荐两款负电压芯片,包括开关负电压芯片和线性负电压芯片,这两款的输入为-24至-10V,输出为-15V至-5V,麻烦了,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
LDO可以选择TPS7A3001: http://www.ti.com.cn/product/cn/tps7a3001, -20V以内选择TPS7A3401:http://www.ti.com.cn/product/cn/tps7a3401
你好,
请问你板上有没有正电压电源?如果有可以用tps84259,或者根据http://www.ti.com.cn/cn/lit/an/slva317b/slva317b.pdf 做出正压转负压开关电源。如果需要低纹波,请在后面接负压LDO.
谢谢您,我的板子上有正电源,我看看你给指出的电源芯片,谢谢!
Hi
较小的输出电流,可以用TPS5430系列的1A输出版本TPS5410, 如果对Nosie, 纹波要求非常高,可以再加高PSRR的LDO.