This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

反激电源多路输出问题解决

各位好我的电路输出要求为5V500MA 24V/0.6A 用的是top245 5v做反馈 当5V加满载的时候 24V的电压会上升30V 请问这该如何解决?谢谢

  • 1、多路输出如果只稳一路,要以功率大的一路做反馈,因此你这个应该以24V输出做反馈,而不是5V输出。

    2、多路输出要考虑交叉调整率的问题,如果你5V输出要求精度高,建议稳24V输出,将5V输出抬高到6-7 V,然后通过LDO降压后得到稳定的5V。

  • 楼上正解,

    如果电路已经做出来,可以通过下面方法优化一下24V的调整率。

    一、选择低损耗的器件,尤其是晶体管和二极管,提高主路5V的效率。

    二、在24V输出口接一个1KΩ-5KΩ的假负载。

    通过以上的方法虽然无法实现任何情况下稳压24v,但是能使电压偏离幅度小于原来的30V,改善调整率。