This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3404MR/NOPB在低温下产品不能起动

在12V输入时,能快速启动带动9V ,电流800mA的LED负载,不会出现启动时LED闪烁的情况,这个正常,

但是在输入14V或更高时,启动时输出不稳定,导致LED闪烁,有时甚至无法带动9V,电流800mA的LED负载。

另外,在低温-5℃时,输入12V/14V都无法启动,无法使得LED点亮,这是目前的主要问题点,我们在输入部分直接通过DC SUPPLIY 供电给IC( PIN8& GND),

现在ELSS产品有问题,HAL需要确认93115072相关特性

此IC 仍然不能工作,我们现在怀疑是不是你们供的芯片是不是有品质上0572.93109375-0000_4.pdf的问题,请尽快让你们技术工程师和我们直接电话会议沟通,避免误解。

  • Hi

       电路上L2可以不要,但是C1要尽量靠近Vin脚。  layout上功率回路需要尽量小。 

       原因是高压芯片电感的峰值电流会更大,更容易促发过载保护。layout上功率回路影响过载,电感饱和也会造成过载,都需要确认。

       低温下异常,可以先将Vcc电容加大一点点看看?