Other Parts Discussed in Thread: LM5148
在低温-40℃启动时,出现LM5148概率性工作异常情况。
异常时,测量输出3.3V虽然有,但后级系统起不来,然后测量HO、LO,发现很久才会起振一下,只有个小尖峰。如下图

然后异常后,将LM5148的EN拉低一段时间再拉高后,系统就能正常启动了。
怀疑是不是LM5148进入了Standby或其他工作模式,导致输出异常?
望回复,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在低温-40℃启动时,出现LM5148概率性工作异常情况。
异常时,测量输出3.3V虽然有,但后级系统起不来,然后测量HO、LO,发现很久才会起振一下,只有个小尖峰。如下图

然后异常后,将LM5148的EN拉低一段时间再拉高后,系统就能正常启动了。
怀疑是不是LM5148进入了Standby或其他工作模式,导致输出异常?
望回复,谢谢!
Hi
将电路传上来看一下.
其次EN信号是系统给的吗? EN是外控信号,需要确认控制源是否异常的导致了EN的输出异常?
HI
确认一下MCU输出EN信号是否因为MCU这边的异常导致EN不稳定? 直接测试EN信号。
如果怀疑时序,你可以直接波形确认:看看EN, VIN等等。