Other Parts Discussed in Thread: TPS62130A
FAE您好:
TPS54335A作数控电压源,用PWM注入FB网络实现数控调压,输入电压12V,输出电压3V-9V,输出电流0.5A-2.5A。
请FAE帮审核原理图设计是否正确?
电压跟随器是否能省掉?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
运放跟随器可以不要的,将PWM通过RC滤波成直流再通过电阻给到FB是可以的。但是不建议你用这款外部补偿的芯片,因为固定的补偿对应固定的输出,可以小范围的变化,一旦输出变化范围偏大,可能导致环路不稳定。
你可以选择TPS62130A这类不需要外部补偿的电路。