Part Number: BQ24650

电路设计如上图,把检流电阻改为20mΩ,电感改为10uH,充电正常,把检流电阻改为4mΩ,电感改为3.3uH时,充电异常,状态1灯有频率的闪烁,电路好像一直在做开关,输入电源为27.2V,2.1A,电感饱和电流为14A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ24650

电路设计如上图,把检流电阻改为20mΩ,电感改为10uH,充电正常,把检流电阻改为4mΩ,电感改为3.3uH时,充电异常,状态1灯有频率的闪烁,电路好像一直在做开关,输入电源为27.2V,2.1A,电感饱和电流为14A
您好,
您请看您右边的bat,您的输入电源支持57.12W 的功率。但是您请求的充电功率最大为25.2V x 10A 或252W。即使在18.6V 的 LOWV 下,仍会请求186W 的输出功率。换句话说,您的输入无法支持输出。因此,输入电压可能会降至 MPPSET 引脚以下,从而停止充电以再次上升,然后再次失败。您选择的 MPPSET 电压显示为6.84V。在此电压下,输入将限制充电电流,以将此引脚保持在6.84V。