Part Number: LM25116
Other Parts Discussed in Thread: LM61495, LM3150
Hi TI team:
项目有个需求是27V DC输入,需要输出3.3V(3A)~12V(10A)的可调输出,请问用什么DC芯片推荐下;
备:已用LM25116配合可调电阻满足此需求,在输出12V 8A负载下 MOS管发热量巨大(120℃)MOS管型号IRFH5006TRPBF;想找到更优的芯片方案
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
不建议选择LM25116, 原因是这个芯片采用外部补偿, 如果要输出可调,不建议范围过大,原因是固定补偿对应固定的输出电压,小范围调节可以,偏离过大可能导致环路不稳定的情况。 建议采用LM3150, LM61495之类的芯片.
如果你已经选用LM25116, 设计时补偿电路对应8V左右,并且在调节范围内,纹波符合需求。 出现MOS发热严重的情况,建议你选择Qg, Rdson尽量小的MOS, 同时注意layout上MOS的散热设计。