This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电源管理

Other Parts Discussed in Thread: LM5022, LM5013, TPS54331, LM5010

您好:

  现在在做一个新案子,需要电源IC,请帮忙推荐下,谢谢!

输入电源:24V 3A

输出电源:18V 1A  & 15V 0.5A  & 10V 0.5A  & 7.5V  0.5A  & 5V  0.5A 

请帮忙推荐下合适的电源IC,谢谢~~~~~