Other Parts Discussed in Thread: LM5022, LM5013, TPS54331, LM5010
您好:
现在在做一个新案子,需要电源IC,请帮忙推荐下,谢谢!
输入电源:24V 3A
输出电源:18V 1A & 15V 0.5A & 10V 0.5A & 7.5V 0.5A & 5V 0.5A
请帮忙推荐下合适的电源IC,谢谢~~~~~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
选择TPS54331D这类的是否可以,电路是不是相对简化一点
24V转成小电压的,用Boost不合适吧
HI
LM5022做成反激,这个隔离的方案。并非要做成boost。
用变压器,多几个绕组,就可以同时做出多路输出。一般4路,额外路选择电流小或者压差小的,可以用LDO或者DC/DC来实现。
HI
没有类似多路输出的推荐方案, 但是以前网站上是有的,现在TI提供的参考设计基本上都是单路输出。(而多路输出,不过就是在单路输出的基础上,变压器多做几个绕组来输出而已)
如果选择LM5010或LM5013之类的是否可行,或者我选择TPS54331, 不用变压器,是不是你之前提及的就不具备隔离功能了?
Hi
是的,你说的这些芯片都是非隔离的,并且你需要5个输出,也就是要用5个芯片来做。 而用LM5022之类反激设计,是隔离方案,需要用到变压器,同时可以做到多路输出。