TI E2E 英文论坛海量技术问答的中文版全新上线,可点击相关论坛查看,或在站内搜索 “参考译文” 获取。

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ769142: PROTECTIONS_RECOVERY_TIME 設定疑惑

Part Number: BQ769142

你好,

想了解 RECOVERY_TIME 的用法,

目前Cell 電壓2.7V 觸發 Cell Undervoltage Protection(電壓:3V) 的保護,當Cell 電壓回復到 CUV_RECOVERY_HYSTERESIS(電壓:3.2V) 時,希望延遲3 second 後將保護解除,

在PROTECTIONS_RECOVERY_TIME 設定為3 second ,意思當達到CUV_RECOVERY_HYSTERESIS 時3 second 後會解除保護?

如果也要設定OCC_THRESHOLD 觸發後 30 second 將 Overcurrent in Charge Protection 的保護解除(不靠電流偵測解除,而是要透過時間來解除保護)

PROTECTIONS_RECOVERY_TIME 在 Cell Undervoltage Protection已經設定為3 second,在Overcurrent in Charge Protection 的PROTECTIONS_RECOVERY_TIME 要如何設定呢?

  • 您好,CUV recover满足下面的条件才会recover:

    Safety Status A()[CUV] = 1 and Min cell voltage > Protections:CUV:Threshold + Protections:CUV:Recovery Hysteresis for Protections:Recovery:Time

    OCC保护恢复条件如下:

    The device will recover (if configured for autonomous recovery) when the voltage measured on the PACK pin falls at least Protections:OCC:PACK-TOS Delta below the voltage measured at the top-of-stack for a duration of Protections:Recovery:Time, or a current less than or equal to Protections:OCC:Recovery Threshold (that is, a discharge current) is present for a duration of Protections:Recovery:Time.

  • 您好

    有看到先前有人的提問及回覆中,

    https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1000337/bq76952-protection-occ-recovery-threshold

    Matt Sunna 最後一個回覆有提及到將discharge current 設定為正值,就會藉由Recovery:Time 來進行恢復。

    CUV 跟 OCC 的恢復時間在文件資料裡都是寫Protections:Recovery:Time,而不像Overcurrent in Discharge,有專用 OCDL:Recovery Time 的設定,所以在Protections:Recovery:Time 設定為3s,那OCC recover 在Protections:Recovery:Time 想要設定為30 second,需要如何設定?

    再麻煩幫忙解答,感激不盡!!!