Other Parts Discussed in Thread: BQSTUDIO
采集化学ID遇到这个问题?
The following errors were reported by the calculation engine:
Error: Discharge current should be negative. No negative current detected in file min current = 0 0
哪位大佬知道怎么解决?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
采集化学ID遇到这个问题?
The following errors were reported by the calculation engine:
Error: Discharge current should be negative. No negative current detected in file min current = 0 0
哪位大佬知道怎么解决?
您好!我测试3串锂电池串联,一串满充是4.2V,容量是2500mAH,我在BQSTUDIO的Calibration中Current设计了-250mA,但是收集到的数据是0,这是怎么一回事?
好的,谢谢!可以给我解惑吗?用1A这是为什么呢?我也测过单个电芯,然后设置还是那样,收集到的电流数据有正有负的?
就是这个收集到的,以0.25A放电
您好!我就是这样设置,但是检测出来的电流数据要不就是一直是250,要不就是一直为0,我不知道是我哪里设置有问题?

放电时候就是一直为0,但是我也挂上了负载
好的,我试试看
您好,请问是哪一篇?
您好, 在下面的帖子中看到校正问题已经解决