This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC5870QDWJEVM-026: UCC5870QDWJEVM-026

Part Number: UCC5870QDWJEVM-026


我将UCC5870供电,12V和5V,并将配套的MCU接在了5870的开发板上,但是MCU的指示灯没有亮,VCC部分也没有供电,上位机软件也检测不到5870,换了两块板子都不行, 无法通过MCU与上位机相连控制UCC5870.想请教一下是什么问题。

  • Hi

        UCC5870只是驱动芯片,确认一下供电是否正常?(可以对照一下datasheet上的电路,确认一下供电是否正常?)

        如果都没有问题的话,再确认一下是否有驱动输入?

  • 谢谢您的回复。我的意思是MCU不知道出什么故障了,上位机根本检测不到连接了MCU,UCC5870的板子没有问题,而且我用了两块MCU,都是新的,现在都连接不上上位机,之前有出现过这种MCU连不上的问题吗?