This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54560B-Q1: 当输入电压小于设定的输出电压时,电源芯片可否正常工作?芯片寿命是否受影响?

Part Number: TPS54560B-Q1
Other Parts Discussed in Thread: TPS54560B, TPS54560

将TPS54560B的输出电压设置为12V。当输入电压小于12V时,芯片占空比趋近100%,输出电压值略微小于输入电压值。

请问在输入电压小于12V,大于4.5V的时候:

1. TPS54560B输出可否达到标称5A输出电流?

2. 长时间工作在这种输入电压小于设定电压的情况,会不会影响电源芯片的寿命?

3. 在这种情况下,输出纹波会不会恶化?

多谢~

  • HI

        首先需要说明的是,TPS54560是一款降压芯片,芯片要正常工作,输入必须大于输入一定电压。只要在“BOOT to SW pin voltage is greater than 2.1 V”才会100%duty。

    所以不建议出现低于12V输入的情况(可以根据datasheet  第12页计算出最小输入电压)。

        如果出现低于上述计算Vinmin的情况,芯片输出会偏低,这种情况实际芯片是不正常工作的,只能通过测试来确认是否符合你的应用。通常不会影响使用寿命。