请问有没有频率大于50Mhz,驱动电流大于30ma的电平转换芯片
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
根据初步筛选,以下器件可能满足您的要求,包括速率、输入输出电压,输出电流一般与供电电压有关,在3.3V输出时需要具体打开datasheet看下是否满足要求,下面截图中的输出电流一般是5V输出时的输出电流。

电平转换IC选型链接:
以上是筛选链接,您可以根据具体需求进一步筛选,或者告诉我,我再进一步帮您确认。
TI没有这个型号 SN74LVC82T45,您是需要 SN74LVC2T45 还是 SN74LVC8T245的模型?但是不管哪个型号,TI所有产品的模型都是在其产品主页下面路径中提供,即“设计和开发”-->“设计工具和仿真”中下载,如下截图所示:

SN74LVC2T45 产品主页:https://www.ti.com.cn/product/zh-cn/SN74LVC2T45
SN74LVC8T245产品主页:https://www.ti.com.cn/product/cn/SN74LVC8T245
另外,请确认上面电路图中型号是否您需要的型号?确认后我再具体确认电路连接情况
未通电,然后Va1有输入5v,VccA那边显示2.5v ,不会出现这种状况吗?(不接二极管)
这里意思是指I/O输入信号拉高了VCCA的电压吗?应该不会,SN74LVC2T45内部没有集成I/O到VCCA的钳位二极管,它怎么会影响VCCA呢?
您说的这个现象具体是指哪款产品,具体型号是SN74LVC2T45吗?
我认为加了I/O至VCCA的二极管反而会对VCCA造成影响,因为此时VCCA=0V,若I/O有输入,高于二极管导通电压,二极管会导通,进而电流流入VCCA,如下FAQ解释: