This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2000: 请教TI的工程师,如图所示,是BQ2000datasheet给出的一个充电器的设计参考图(datasheet中的图7),请问图中红圈部分具体是实现啥功能的。

Part Number: BQ2000


  • 您好, Q3 inverts the MOD output so it can drive a PFET.  Q2 is part of Q1 fast turn off circuit.  D7 is Zener clamp to protect gate of Q1 (EVM rated for up to 25V input) but will also help with Q1 fast turn off since the gate is not pulled all the way to ground at turn on.  If you input voltage is low enough not to exceed PFET max gate voltage, then D7 is not required but, again, will help with Q1 turn off time.