This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5069: 关于LM5069的功率设置问题

Part Number: LM5069


Rpwr=1.3x10^5xRsns xPLim;

LM5069的第7脚,我原来是设置150k的,是想着功率设置到最大,让Rsense(=9mR)设定电流(Imax=1.5*4A)而设定了实际功率,

但是这样设置后,一开启负载仪做带负载测试,就即刻会击穿mos;(Nmos的选用的型号是NCEP020N10LL);

之后把LM5069的pin7改为了53K后,不会烧nmos了,也能带载到5.7A;

现在我的问题就是Plim设置的依据是什么?

感谢!