Part Number: LM5069
Rpwr=1.3x10^5xRsns xPLim;
LM5069的第7脚,我原来是设置150k的,是想着功率设置到最大,让Rsense(=9mR)设定电流(Imax=1.5*4A)而设定了实际功率,
但是这样设置后,一开启负载仪做带负载测试,就即刻会击穿mos;(Nmos的选用的型号是NCEP020N10LL);
之后把LM5069的pin7改为了53K后,不会烧nmos了,也能带载到5.7A;
现在我的问题就是Plim设置的依据是什么?
感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM5069
Rpwr=1.3x10^5xRsns xPLim;
LM5069的第7脚,我原来是设置150k的,是想着功率设置到最大,让Rsense(=9mR)设定电流(Imax=1.5*4A)而设定了实际功率,
但是这样设置后,一开启负载仪做带负载测试,就即刻会击穿mos;(Nmos的选用的型号是NCEP020N10LL);
之后把LM5069的pin7改为了53K后,不会烧nmos了,也能带载到5.7A;
现在我的问题就是Plim设置的依据是什么?
感谢!
HI
按照datasheet里的设计案例来做,具体可以参照datasheet 20页9.2.1.2.3 Select Power Limit
HI, Johnsin Tao
Plim_min=(Vsns_min*Vin_max)/Rsns,这个公式是限制电路启动瞬间的功率?还是限制了电路的工作功率?