This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2842A: 原輸出12V/60W,變更為5V/50W

Part Number: UC2842A


Hi all....

如題,原變更壓匝比 PRI:SEC:AUX為 40:6:7,僅變更輸出繞組匝比為 40:2.5:7,輸出反饋參數調整輸出5V正常。

但PWM IC VCC引腳(AUX繞組) 輕載時11V~12V正常,一抽載約至0.4A, IC VCC引腳電壓就拉升接近30V,

再拉高抽載VCC電壓就超過極限值了!

試過調整Sunbber電路、RT頻率(原70KHz)、加大輔助繞組串聯電阻等,皆無明顯改善,想請問線路問題出在哪?