我采用LM2840YMK将28V转为12V,电路原理图如下图所示:

测试中遇到的问题1)如下:产品断电时,当28V下降到6v左右时,LM2840会异常启动,是什么原因?当我把负载电流增大后,此现象消失。断电时波形如下。


问题2)续流二极管D1选择一般的快恢复开关管和肖特基管有什么区别,我分别采用2CK78DUR和1N5819都试过,就恢复时间两者差的不多(10ns、5ns)应该都可以。另外手册中SW信号要求最小值为-0.3V,这个是必须的么?为什么?即使采用肖特基二极管,在大负载的情况下也无法做到导通压降小于0.3V。特别在启动时,一般电流较大,SW均可能低于-0.3V。我测试结果来看,采用肖特基的稳态裕度大些,采用2CK78DUR时负载大于35mA时易造成LM2840故障,采用1N5819-1时负载在60mA时均可正常工作,LM2840在此负载增大的情况下可能是什么原因故障的?随着负载增大,可以看到12V上电流出现20mA的毛刺尖峰。
问题3)lm2840对输入电压上升斜率是否有要求,我测试发现如果直接28V上电,LM2840极易损坏,若软启动则不会。
问题4)电感L1若选择的较小,有什么危害么,还是仅仅工作在非连续模式,如果对12V稳定性要求不高,是否可以减小电感?
问题5)测试发现SW信号在LM2840Y导通时电压尖峰很高如下图所示,改为LM2840X后明显减小,是由于电感距离LM2840较远造成的么?更换二极管D1无作用,减小电感L1是否会减小此电压尖峰?

问题6)由于布局限制,电路中电感L1距离2840等其它器件较远,且在电路板的不同面,请问对电路的影响包括哪些方面,可能造成什么后果?在不改变电路布局的情况,可以通过改变电容改善么?