两个直流12V电源分别接2个LM5050-1,工作电流1.5A,我们设计初衷是考虑正常情况下只有一个电源供电,在这个电源突然断电的情况下,另外一路可以无缝衔接上,现在测试情况是,两路电源都有电流输出,一个多点一个少点,MOSFET用的是SI4840BDY,请问这种情况正常吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
两个直流12V电源分别接2个LM5050-1,工作电流1.5A,我们设计初衷是考虑正常情况下只有一个电源供电,在这个电源突然断电的情况下,另外一路可以无缝衔接上,现在测试情况是,两路电源都有电流输出,一个多点一个少点,MOSFET用的是SI4840BDY,请问这种情况正常吗?
Hi
这样用是可以的,采用2个电源通过oring电路来控制。
至于2个电源都有输出,你需要确认2个电源的输出是否来自电源还是电压反灌?
我是用2个稳压电源模拟供电,输出接直流负载,从电源显示上看,2个电源工作电流和正好等于负载电流。
HI
看起来是正常现象,因为你两路输入是一样的电压。
现在怀疑导致电源模块损坏的原因是其中一路模块输入突然断开,LM5050-1的反向保护没有起作用,另一路模块倒灌回去,导致这个模块损坏,有没有可能是这个原因?
HI
有可能的,只要LM050控制的MOS击穿就会出现电压反灌。
正常而言,只会一路电源启动, 你可以关掉其中一路看是否有电流反灌。