This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25890H: BQ25890H主充+BQ25601辅充,cv两颗ic均设置4430mV,iterm主充设置320mA,辅充为默认180mA,主充截至后一秒,辅充也截至了

Part Number: BQ25890H
Other Parts Discussed in Thread: BQ25890, BQ25892

截至后dump的寄存器如下:

<3>[ 5053.502397][T1000244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[00] = 0x11

<3>[ 5053.504183][T1000244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[01] = 0x01

<3>[ 5053.506125][T1000244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[02] = 0x41

<3>[ 5053.507908][T1000244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[03] = 0x1a

<3>[ 5053.509867][T1200244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[04] = 0x1e

<3>[ 5053.511862][T1000244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[05] = 0x14

<3>[ 5053.513736][T1000244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[06] = 0x96

<3>[ 5053.515527][T1000244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[07] = 0x8f

<3>[ 5053.517317][T1000244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[08] = 0x03

<3>[ 5053.519224][T1000244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[09] = 0x4c

<3>[ 5053.521004][T1000244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[0a] = 0x71

<3>[ 5053.570483][T1000244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[0b] = 0x7e

<3>[ 5053.572335][T1000244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[0c] = 0x00

<3>[ 5053.574454][T1200244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[0d] = 0x12

<3>[ 5053.576451][T1000244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[0e] = 0x67

<3>[ 5053.578375][T1000244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[0f] = 0x6b

<3>[ 5053.580160][T1000244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[10] = 0x3f

<3>[ 5053.582254][T1000244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[11] = 0xc9

<3>[ 5053.584047][T1000244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[12] = 0x00

<3>[ 5053.585882][T1000244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[13] = 0x11

<3>[ 5053.587671][T1000244] charger_thread: [bq2589x]:bq2589x_dump_regs: [name:bq2589x_charger&]Reg[14] = 0x1f

<3>[ 5053.589652][T1100244] charger_thread: [bq2560x]:bq2560x_dump_regs: [name:bq2560x_charger&]Reg[00] = 0x68

<3>[ 5053.591648][T1000244] charger_thread: [bq2560x]:bq2560x_dump_regs: [name:bq2560x_charger&]Reg[01] = 0x1a

<3>[ 5053.593522][T1100244] charger_thread: [bq2560x]:bq2560x_dump_regs: [name:bq2560x_charger&]Reg[02] = 0xa0

<3>[ 5053.595333][T1000244] charger_thread: [bq2560x]:bq2560x_dump_regs: [name:bq2560x_charger&]Reg[03] = 0x32

<3>[ 5053.597120][T1000244] charger_thread: [bq2560x]:bq2560x_dump_regs: [name:bq2560x_charger&]Reg[04] = 0x90

<3>[ 5053.599001][T1000244] charger_thread: [bq2560x]:bq2560x_dump_regs: [name:bq2560x_charger&]Reg[05] = 0x8f

<3>[ 5053.600795][T1000244] charger_thread: [bq2560x]:bq2560x_dump_regs: [name:bq2560x_charger&]Reg[06] = 0xe6

<3>[ 5053.602675][T1000244] charger_thread: [bq2560x]:bq2560x_dump_regs: [name:bq2560x_charger&]Reg[07] = 0x4c

<3>[ 5053.604459][T1000244] charger_thread: [bq2560x]:bq2560x_dump_regs: [name:bq2560x_charger&]Reg[08] = 0x3c

<3>[ 5053.606347][T1000244] charger_thread: [bq2560x]:bq2560x_dump_regs: [name:bq2560x_charger&]Reg[09] = 0x00

<3>[ 5053.608128][T1000244] charger_thread: [bq2560x]:bq2560x_dump_regs: [name:bq2560x_charger&]Reg[0a] = 0x83

<3>[ 5053.610005][T1000244] charger_thread: [bq2560x]:bq2560x_dump_regs: [name:bq2560x_charger&]Reg[0b] = 0x11