This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65218D0: TPS65218D0

Part Number: TPS65218D0

数据手册中,DC-DC4这一路,提到一个开关频率fsw=2400Hz,但我用示波器对DC-DC4电源进行纹波测试。发现:(具体数据见报告)
1、未加负载时纹波频率为9.8Khz
2、加上0.05A负载后电源纹波频率在逐渐降低到2.7kHz,
3、当外接负载电流达到0.06A以上,电源纹波频率跃变到100Khz。
所以我的问题;
1、为什么初始频率不是数据手册上的2400Hz
2、开关频率fsw会不会变,如果会变,请问在9kHz这个阶段,芯片是工作在PFM模式/PWM模式