Part Number: TPS74901
想使用TPS74901RGW,实现输入5V,输出3.3V,实际使用电流约1A,外部环境温度最高约50℃,想把Vin和Vbias都接5V,这种接法是否可以?请教

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS74901
想使用TPS74901RGW,实现输入5V,输出3.3V,实际使用电流约1A,外部环境温度最高约50℃,想把Vin和Vbias都接5V,这种接法是否可以?请教

Hi
都接5V没有问题,但是要注意一下散热设计,因为1.7W功耗很大,而且环境温度也很高。