请教一下,如图MOS管Q3 的源极(S)和漏极(D)短接起来,然后将电池输出的正负极进行短路测试,发现Q2的栅极没有高电平,Q2没有处于导通状态,持续短路很快MOS就烧了,这是为什么,IC没有出现掉电,通讯都是正常的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教一下,如图MOS管Q3 的源极(S)和漏极(D)短接起来,然后将电池输出的正负极进行短路测试,发现Q2的栅极没有高电平,Q2没有处于导通状态,持续短路很快MOS就烧了,这是为什么,IC没有出现掉电,通讯都是正常的。
您好,没有击穿,我是做瞬间短路,P+ P-短路的时候Q2的栅极只有8v多,断开短路时Q2栅极有27v。
那这是什么原因?
P+ P-短路的时候Q2的栅极只有8v多,断开短路时Q2栅极有27v,应该是体二极管的原因阻抗会变大。
短路的时候Q2应该是导通的,mos管也测试了是好的,体二极管阻抗变大那断开后能正常恢复。
您好,瞬时短路,断开以后会恢复正常,如果长时间短路Q2会发热,电路上没有FUSE,如果有会熔断,cell端有TCO也会启动保护。
MOS管内的体二极管会导致短路时MOS管不能正常导通?然后烧坏?
您好,您短接的Q3没有损坏吧,没有短接的Q2在短路时会发烫。
Q3是完好的,Q2在短路时会发热,短路时Q2的G极没有高压,为什么会没有高压。
您好,因为短路时MOS会关掉,charge pump会拉底。
您好!ASCD保护时不是只关DSG,,CHG看还是打开的。。。
MOS管Q3 的源极(S)和漏极(D)短接起来,然后将电池输出的正负极进行短路测试,为什么显示CHG是打开的,Q2的栅极只有8V,实际上是不处于导通,这是为什么?
您好,请参考下面内容:
What is the voltage of the PACK+ pin when you observe this behavior? From the image you attached it appears like the gauge is trying to be in charge mode and no protections should be opening the CHG FET. However, BatteryStatus() DSG is still set. I am thinking there may not be enough current flowing for the device to exit relax mode.