This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG1205: 使用方法以及死区问题

Part Number: LMG1205


1:上图是官方图纸,控制PWM死区,但是硬件具体是如何实现的不太理解,可不可以详细讲解一下工作原理,以及PWM死区时间是如何控制的呢?

2:上图是完整图纸,有几个问题问一下,图纸中输入控制引脚HI和LI是一对带死区的反向PWM。

问题1:这个芯片两个输入脚必须同时是PWM吗,可以不是PWM吗?

问题2:如果输入必须是PWM,PWM的占空比有要求吗?最大支持到多少?PWM频率最高到多少?

问题3:如果可以用高低电平控制,比如输入80V,驱动输出也是80V, 设置HI高电平,LI低电平可以实现吗?

问题4:如果输入80V,驱动输出是40V,设置HI的PWM占空比50%,LI低电平可以实现吗?   

问题5:如果输入80V,驱动输出是40V,第一种方式:HI的PWM占空比50%,LI低电平,和第二种方式:HI的PWM占空比50%,LI的PWM反向占空比也是50%, 两种方式效果一样吗?