This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR14020: 输出电流达不到设计的电流值就会保护

Part Number: LMR14020


在设计了LMR14020降压电流后,要求设计输入:18V-36V,输出7V  2A,我按照如下原理图设计,发现输出电流在1.6A就会保护,而且输入电压在28V也会保护,请问是我原理图设计在哪里有问题吗?我通过TI的TINA软件仿真,是没有问题的,但是实际的实物不行,有分析的方向吗?谢谢

其中,电感规格:6.8uh,IR2A,Istat 2.7A,RDC0.059R

          二极管规格:SS54