Part Number: UCC5870-Q1
我使用UCC5870芯片, 用自己做的板子,VCC1为3.3V,VCC2为15V,VEE2为-8V。ASC_EN为3.3V。
现在遇到上电nFLT1为高,nFLT2为低,但是内部寄存器是可以读取的,且数值正确,操作DRV_EN,然后操作IN-和IN+高低变化,但是输出始终为-8V,如果使得ASC引脚为高,那么nFLT1和nFLT2都为低。
请问这种情况应该如何解决?
下图是我的SPI波形

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: UCC5870-Q1
我使用UCC5870芯片, 用自己做的板子,VCC1为3.3V,VCC2为15V,VEE2为-8V。ASC_EN为3.3V。
现在遇到上电nFLT1为高,nFLT2为低,但是内部寄存器是可以读取的,且数值正确,操作DRV_EN,然后操作IN-和IN+高低变化,但是输出始终为-8V,如果使得ASC引脚为高,那么nFLT1和nFLT2都为低。
请问这种情况应该如何解决?
下图是我的SPI波形

Hi
应该是配置上的问题,但是TI没有提供例程以及操作文档说明,建议你在美国E2E上要一下,看是否有可以参考的例程或者操作步骤说明:https://e2e.ti.com/