This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65251: 芯片输出异常

Part Number: TPS65251

新设计了一款主板的方案,其中的电源部分使用了之前曾经验证过的TPS65251的电路,但是板子做回来了之后发现TPS65251无输出,新旧版原理图如下:

新版主要故障现象如下:

  1. 三路输出分别是6.9V -0.5V 0.25V ,并且第一路6.9V只在保险丝接上时有输出,断开保险丝后测量三路均为0V。
  2. V3V引脚输出为0.25V,V7V引脚输出为0.5V,ROSC为100mV左右的非周期信号
  3. 三路的EN脚均为低(0.2V),强制上拉至3.3V也不能正常工作
  4. 修改SS1/2/3的电容值对结果无影响
  5. 更换芯片无效果

用旧版测试,旧版的输出及各引脚状态正常。目前不知道是哪里出现了问题。