This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: MCU和BQ76952进行IIC通讯时,MCU作为主机、BQ76952作为从机,IIC的CLK信号为什么两者都会去控制?

Part Number: BQ76952
Other Parts Discussed in Thread: ISO1541, ISO1540

电路中MCU和BQ76952的IIC通讯进行了隔离,如下图所示:

使用了ISO1541,是单向CLK+双向DATA的IIC隔离芯片,此时IIC通信会失败

换成ISO1540,是双向CLK+双向DATA的IIC隔离芯片,此时IIC通信成功

抓取波形,下图是ISO1541通信失败的波形(黄色是CLK、蓝色是DATA):

抓取波形,下图是ISO1540通信成功的波形(黄色是CLK、蓝色是DATA):

可以看到,通信成功的时候,IIC_CLK有一段时间是被一直拉低的,和通信失败的波形对比发现:拉低CLK的这个动作是由AFE_BQ76952执行的。

那为什么作为从机的BQ76952会拉低CLK呢?

而且拉低的这段时间DATA其实是有数据变化的,那这段时间的数据不就丢了吗?怎么反而通信成功了呢?

(备注:我们使用的是IIC_CRC,不知道带了这个校验是不是有关系?)