This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LC滤波器设计



图不知怎么显示出来,大家看附件吧
变器输出采用LC滤波,如图
8 LC滤波电路
输出滤波电感的最小值由设定的电感电流纹波决定,一般取15%20%的额定电流。本设计中取20%,在220V/3kVA下设计得到,
   
下面计算电感量,
                      3-1
根据单极性SPWM原理,因为开关频率远大于工频频率,所以得到
                   3-2
                                3-3
如果对于双极性SPWM的设计,需要注意和上式有所不同,
               3-4
                           3-5
因为本设计采用单极性,所以每个开关周期的占空比为:
                              3-6
将(3-6)式代入(3-1)式得
                        3-7
所以,当 时,有最大值,
                                3-8
                                                 3-9
代入VDC=380VfS=20kHz =2.727A得:
                   3-10
L = 2.0mH
然后设计电容C
电容和电感构成LC低通滤波器,频率高于其谐振频率的高次谐波将以40dB/decade衰减,所以其谐振周期设计为5~10倍的载波周期,本设计取10
               3-11
带入数据得:
C = 3.3uF

 
LC滤波器设计.doc